NTN Exhibits at “Tokyo Motor Show 2013”November 19, 2013
| Date |
November 22 (Fri) to December 1 (Sun), 2013 |
| Venue |
Tokyo Big Sight |
| NTN Booth |
East Hall E5101 |
NTN will run an exhibit at “Tokyo Motor Show 2013” with the theme “NTN’s Overriding Technologies Support the Future of Vehicles.”
The NTN booth will feature next-generation EV system products and other module products designed with electrification in mind, as well as a wide range of products that contribute to better efficiency and lighter weight of vehicles.
The stage within the booth will be used for the “Q’mo II” two-seater electric commuter concept car equipped with NTN’s EV systems to demonstrate its “Pivot turn” and “Lateral move” functionalities. Be sure to check out the impressive visuals combined with the characteristic Q’mo moves.
We look forward to seeing you at the event.
Main exhibits
|
The two-seater commuter “Q’mo” created a major stir at last year’s Tokyo Motor Show. It has been further improved for city driving, whilst maintaining the unique “Pivot turn” and “Lateral move” functionality of the In-wheel Motor System. Watch the stage come alive with movement that no other vehicle can imitate. |
 |
|
An EV system product featuring the world’s lightest class in-wheel motor that can be mounted directly within a wheel and equipped with a cycloid reducer mechanism, hub bearing and various sensors, and includes a control system consisting of an inverter. Mounting the motor directly to the wheel allows more effective use of free space and greater design flexibility for vehicles. |
 |
|
The technology of steering system for steer-by-wire that changes the steering angle to the appropriate electrical signal to drive the wheel-turning actuator, and changes the direction of the tires (wheel-turning) has been specially developed for rear wheel applications as a reference exhibition. An integrated system controls both sides to steer the rear wheels, and also allows control of the toe angle to contribute to better driving performance. |
 |
|
A compact drive module that combines support bearings, sintered materials and other components with high load capacity ball screws. The drive module converts motor rotation precisely to straight line motion, and finely adjusts the braking force for greater regeneration of drive energy to contribute to cruising distance. |
 |
|
A thin and lightweight module product designed for CVT and the electrification of various other actuators. The use of a ball screw with minimal rolling resistance helps to reduce drive force and electrical force losses due to pulley operation. The hollow screw shaft can be positioned along the same shaft as the pulley shaft to make CVTs more compact in size. |
 |
|
Hub joint that uses a proprietary pressed connect method for a lightweight design and no backlash in spline joints. The bolt connection structure between the CVJ and 3rd generation hub bearing makes assembly possible on the vehicle production line. |
 |
High Performance Deep Groove Ball Bearing for Transmission
This high thrust load deep groove ball bearing drastically improves thrust capacity by optimizing the shape of bearing ring groove and employing a newly designed assembly cage, integrated with a seal that self-forms minute gaps between the inner ring and seal. The bearing also features special heat treatment technology to improve anti-indention, and is capable of replacing tapered rolling bearings for major reductions in torque. |
 |
Social demonstration vehicles used in Japan and France also on show
Social demonstration projects are being conducted around the world using electric commuters equipped with the In-wheel motor with the aim of accelerating development of advanced technology and faster uptake of EV and next-generation vehicles.
Vehicles used in social demonstration projects in Japan and France will be on show at the booth. |
 |
Inquiries about this release