HOME > News > Press Releases : 2013 > Public Road EV Demonstration Project of Microcompact EV Equipped with In-wheel Motor

2013

Print

Public Road EV Demonstration Project of Microcompact EV Equipped with In-wheel MotorAugust 9, 2013Press Releases

[Unveiled at “Mt. Fuji EV Festa” held in Shizuoka Prefecture]

NTN Corporation (hereafter, NTN) has started a public road EV demonstration project by unveiling the first microcompact, two-seater electric vehicle (EV) equipped with NTN's own “In-wheel Motor System” registered as a light vehicle in Japan on August 1 at “Mt. Fuji EV Festa”.

Mt. Fuji EV Festa was held as part of efforts to increase awareness of environmental conservation activities following the registration of Mt. Fuji as a world heritage site, as well as the “Fujinokuni EV/PHV Town Concept” initiative organized by Shizuoka Prefecture with the aim of popularizing EVs. The microcompact, two-seater EV equipped with NTN's In-wheel Motor System acquired a light vehicle registration number following further development and testing after it was driven during the opening ceremony*1 of the New Tomei Expressway in April last year. Shizuoka Prefectural Governor Kawakatsu rode in the EV as it took the role of lead parade vehicle in “Mt. Fuji EV Festa” on August 1.

In January this year, NTN successfully completed a social demonstration test*2 of the In-wheel Motor System for modified electric vehicles (converted EV) over approximately one year with the cooperation of Iwata City in Shizuoka Prefecture, Japan, while a demonstration project*3 began from June in collaboration with Annecy City in France (where the NTN-SNR head office is located) after acquiring official certification for electric microcars in Europe.

NTN has utilized the technology it has gained through research and development into bearings, as well as maximized the strength of the world's No. 1 share in hub bearings to advance development of the In-wheel Motor System and other system products for next-generation vehicles such as EVs and environmentally friendly vehicles. Conducting demonstration projects in Japan and Europe, where development and business plans for next-generation vehicles are more advanced, will help accelerate development and business plans of cutting-edge technology designed for the commercialization of EV system products, while also increasing the number of activities designed to popularize the microcompact mobility more quickly.

*1 New Tomei Expressway opening ceremony

*2 Converted EV demonstration project in Iwata City

*3 Demonstration project in Annecy City, France

Photo: “Fujinokuni EV, PHV Town Concept” by Shizuoka Prefecture“Fujinokuni EV, PHV Town Concept” by Shizuoka Prefecture

Photo: The microcompact, two-seater EV equipped with the In-wheel MotorThe microcompact, two-seater EV equipped with the In-wheel Motor

Microcompact, two-seater EV (Public Road Demonstration Vehicle)

Photo: Microcompact, two-seater EV (Public Road Demonstration Vehicle)NTN's In-wheel Motor/EV Module Development Business in based on Iwata City, Shizuoka Prefecture.
The vehicle was produced by Tajima Motor Corporation in Iwata City.

[In-wheel Motor System for Compact EV]

■Features of the In-wheel Motor System for Compact EVs

-Effective use of free space and greater design flexibility-

  1. Compact in-wheel motor module A thin hub bearing has been used, allowing it to be mounted within the wheel.
  2. Drivetrain integrated into a systemized unit Drive motor, reducer, hub bearing, control system (including inverter)
  3. Independent control of drive power to left and right wheels

Photo: In-wheel motor system for compact EVsIn-wheel motor system for compact EVs

Photo: Compact, two-seater EV (chassis model)/Installed in the rear two wheels

Compact, two-seater EV (chassis model)

Installed in the rear two wheels

Scenes from Mt. Fuji EV Festa

Photo: Greetings by Shizuoka Prefectural Governor Kawakatsu at the opening ceremonyGreetings by Shizuoka Prefectural Governor Kawakatsu at the opening ceremony

Photo: Shizuoka Prefectural Governor Kawakatsu (left), Chairman Fukutake of the Association for the Promotion of Electric Vehicles (center) and Chairman Tajima of Tajima Motor Corporation (right)Shizuoka Prefectural Governor Kawakatsu (left), Chairman Fukutake of the Association for the Promotion of Electric Vehicles (center) and Chairman Tajima of Tajima Motor Corporation (right)

Photo: Shizuoka Prefectural Governor Kawakatsu (right) and Chairman Tajima of Tajima Motor Corporation (left)Shizuoka Prefectural Governor Kawakatsu (right) and Chairman Tajima of Tajima Motor Corporation (left)

Photo: Governor Kawakatsu and Chairman Tajima (winning driver of the Pikes Peak International Hill Climb in July) before departing in the lead parade vehicleGovernor Kawakatsu and Chairman Tajima (winning driver of the Pikes Peak International Hill Climb in July) before departing in the lead parade vehicle

Photo: “Converted EV equipped with the Onboard Drive System” driven as the follow-up parade vehicle“Converted EV equipped with the Onboard Drive System” driven as the follow-up parade vehicle

Photo: “Converted EV equipped with the In-wheel Motor System” that was used for test drives“Converted EV equipped with the In-wheel Motor System” that was used for test drives

Inquiries about this release

Inquiry Form

Print