NTN Exhibits at China's Largest International Trade Fair for Construction Machinery “bauma China 2014”November 17, 2014
| Date | November 25 (Tue) to 28 (Fri), 2014 |
|---|---|
| Venue | Shanghai New International Expo Centre Shanghai, China |
| Booth No. | N1.476 |

NTN will run a booth at China's Largest International Trade Fair for Construction Machinery “bauma China 2014” with the theme “Proposing the state-of-the-art technology — Passing on technology to the next generation and ongoing development.”
The booth will feature exhibits of the ULTAGE*1 series spherical roller bearing, as well as large size tapered roller bearing and Filter Seal Integrated Large Size Bearing to propose longer operating life and more compact in size. Other exhibits will include the IC Tag Integrated Bearing, Integrated Rotation Sensor Bearing and angle sensor unit that utilize sensor technology, as well as maintenance tools and other products for the aftermarket.
A model hydraulic excavator will be set up in the center of the booth to show the different bearings being used in each area, and cutaway models will also be used to provide information on products.
We look forward to seeing you at the event.
| *1) | ULTAGE is the name for NTN's new generation of the world's highest standard of bearing series, and expresses the “ULTIMATE” performance on any type of “STAGE.” |
Main exhibits
ULTAGE series of rolling bearings for construction machinery 

IC Tag Integrated Bearing
The industry's first product that allows information to be recorded and read with an IC tag built into the bearing and a special reader/writer unit. The type of information saved can be configured for each user, allowing bearing quality information, as well as inspection records, to be checked.

Filter Seal Integrated Large Size Bearing
Prevents penetration of foreign matters within lubricant into the bearing to extend the bearing replacement interval. The filter seal has been incorporated without changing the outer dimensions of the bearing, which allows replacement of existing bearings.

Maintenance tools