Clutches
Clutches

Mechanical element that controls the transmission and interruption of rotational force. Includes the one-way clutch which only drives in one direction and is idle in the reverse direction, the two-way clutch which is capable of switchover between drive and idle modes in both directions, and the torque diode where the output shaft also rotates if the input shaft is rotated.
- Related Catalog