HOME > News > Press Release : 2025 >  NTN's Transportable Independent Power Supply “N3 N-CUBE” Helps Prevent Heatstroke Providing Cool Air with 100% Renewable Energy

2025

NTN's Transportable Independent Power Supply “N3 N-CUBE” Helps Prevent Heatstroke Providing Cool Air with 100% Renewable Energy July 22, 2025 Press Release

  • Used as an air-conditioned rest area at “THE ROAD RACE TOKYO TAMA 2025,” an international bicycle road race
  • Promoting as a “cooling shelter” for heatstroke prevention as well as emergency power supply in the event of disasters

Transportable Independent Power Supply “N3 N-CUBE” developed by NTN Corporation (hereafter, NTN) was utilized as an air-conditioned rest area at “THE ROAD RACE TOKYO TAMA 2025,” an international bicycle road race held in the Tama district (Western Tokyo), Japan on July 13. It was installed to help prevent heatstroke and ran air conditioning and lighting with electricity generated from wind and solar power to create a cool and comfortable space.

“N3 N-CUBE” stores a compact wind turbine, solar panels, and storage batteries in a container, and features high mobility as it can be easily transported by means such as truck. The inside of the container can be customized. In normal times, it can be used as an eco toilet, bus stop, or rest area. During disasters, it can be transported to areas that need electricity and start generating and supplying power immediately.

As natural disasters like typhoons, heavy rain, and earthquakes occur frequently, power outages have become a major issue. Many local governments are now adopting this product as it can be used both in normal times and during emergencies.

“N3 N-CUBE” used at this event was sold by NTN to a company in Sakurai City, Nara Prefecture, Japan. It is equipped with air conditioning, lighting, desks, and chairs. To ensure the safety of event staff during the hot summer, the company offered the unit for the race, and it was used as a rest area at the venue.

On the day of the race, the temperature exceeded 30°C (about 86°F). The air conditioning, powered by 100% renewable energy, provided a cool and comfortable space, helping to prevent heatstroke.

Due to global warming, heatstroke prevention has become a serious social issue. Last year, Japanese government enforced a revised climate change adaptation act. When special heatstroke alert is issued due to high temperatures, public facilities like community centers and libraries, as well as designated companies' facilities, will be opened as “cooling shelters.”

NTN is actively promoting the “N3 N-CUBE” as a cooling shelter that runs on 100% renewable energy and can also serve as a backup power source in the event of disasters in Japan.

As awareness of disaster prevention grows in Japan, there is a movement to use roadside stations as disaster response hubs. In April last year, the Ministry of Land, Infrastructure, Transport and Tourism issued guidelines for using high-value containers at roadside stations to support both local revitalization and disaster response. We also have been focusing on proposing the “N3 N-CUBE” for these disaster prevention roadside stations*1, aiming to help create safe and secure communities.

  1. Press release on October 9, 2024:
    NTN Has Held Demonstration Test for Transportable Independent Power Supply “N3 N-CUBE” in the Event of Disasters
    https://www.ntnglobal.com/en/news/press/news202400082.html
Photo:“N3 N-CUBE” installed as a rest area “N3 N-CUBE” installed as a rest area
Operating air conditioning and lighting by using
rooftop solar panels and a compact wind turbine
Photo:Utilized as relaxing rest area with desks and chairs installed inside Utilized as relaxing rest area with
desks and chairs installed inside

Use examples of Transportable Independent Power Supply “N3 N-CUBE”

ApplicationEco toilet ApplicationFlood prevention center ApplicationDisaster prevention warehouse ApplicationBus waiting area ApplicationRecharging station ApplicationWorkation
LocationKuwana City and Matsusaka City, Mie Prefecture, Japan LocationYoshida Town, Shizuoka Prefecture, Japan LocationKuwana City, Mie Prefecture, Japan LocationYoshida Town, Shizuoka Prefecture, Japan Location- LocationSakurai City, Nara Prefecture, Japan
Photo:Eco toilet(Kuwana City and Matsusaka City, Mie Prefecture, Japan) Photo:Flood prevention center(Yoshida Town, Shizuoka Prefecture, Japan) Photo:Disaster prevention warehouse(Kuwana City, Mie Prefecture, Japan) Photo:Bus waiting area(Yoshida Town, Shizuoka Prefecture, Japan) Photo:Recharging station Photo:Workation(Sakurai City, Nara Prefecture, Japan)
Equipped with a circulating flush toilet with treatment tank Can be installed without water and sewage infrastructure Equipped with air conditioning and lighting Functions as a disaster prevention base Can control temperature 24 hours a day by installing air conditioners Equipped with air conditioning, lighting, power outlets, Wi-Fi, and chairs Supplies electricity to personal mobility devices like e-bikes and scooters, and vending machines Ensures mobility in tourist areas and during disasters Equipped with air conditioning, lighting, desks, and chairs Can be used as a cooling shelter for heatstroke prevention

Inquiries about this release

Inquiry Form

Print