HOME > Product and Technology > Products News : 2026 >  Strengthening Communications and Disaster-Prevention Infrastructure on Remote Islands NTN Signs Comprehensive Partnership Agreement with Taketomi Town, Okinawa

2026

Strengthening Communications and Disaster-Prevention Infrastructure on Remote Islands
NTN Signs Comprehensive Partnership Agreement with Taketomi Town, Okinawa
July 31, 2026 New Products

  • Aiming to Build a Remote-Island Infrastructure Model That Remains Operational during Disasters Using the Renewable-Energy-Powered “N3 N-CUBE”

NTN Corporation (NTN) and Taketomi Town, Okinawa, have entered into a comprehensive partnership agreement aimed at promoting sustainable community development and addressing challenges specific to remote-island communities. A signing ceremony was held on July 21 at Taketomi Town Hall in Ishigaki City, Okinawa. Through this agreement, the parties will work to address challenges related to disaster-prevention, communications, and daily-life infrastructure in remote islands using NTN's Transportable Independent Power Supply “N3 N-CUBE,” which operates solely on renewable energy.

Taketomi Town consists of multiple remote islands, including Iriomote Island and Taketomi Island. The municipality faces various challenges, including limitations in social infrastructure such as electricity, water and sewage systems, and telecommunications, as well as the need to strengthen disaster preparedness and accommodate a growing number of tourists. In May 2025, NTN installed the “N3 N-CUBE” Restroom Model on Iriomote Island. The model combines a transportable independent power supply that operates solely on renewable energy with a self-contained circulation type flush toilet system. It can be deployed in locations where power, water supply, and sewage infrastructure are difficult to establish, contributing to improved convenience for both residents and tourists.

Under this agreement, the initiatives already underway on Iriomote Island will be expanded throughout Taketomi Town. In addition to enhancing the convenience of daily-life infrastructure using “N3 N-CUBE”, NTN and Taketomi Town aim to establish an inter-island communication network supported by independent power supplies that remain operational during power outages and disasters. Going forward, demonstration projects and the necessary preparations for implementation will be carried out to help ensure the safety and security of residents and tourists while promoting sustainable community development throughout the remote-island region.

At the signing ceremony, Taketomi Town Mayor Masato Maedomari commented:

“Securing accurate information is one of the most important priorities during disasters. Through this agreement, we aim to advance the development of an inter-island communication network and foster a community where residents and tourists alike can feel safe and secure.”

He expressed his expectations for the agreement.

Hideki Umemoto, General Manager of the Green Energy Products Unit, Innovation & Business Development HQ of NTN, stated:

“We will continue to expand the initiatives that began on Iriomote Island throughout Taketomi Town and work together with public and private stakeholders to address regional challenges through the deployment of independent power supplies and communication networks using N3 N-CUBE.”

He also expressed his commitment to co-creating solutions with local communities and helping address challenges unique to remote-island regions.

NTN will further promote the deployment of “N3 N-CUBE” through collaboration with local governments and communities, contributing to the resolution of regional challenges and the realization of a sustainable society.

Photo:Comprehensive Partnership Agreement Signing Ceremony Comprehensive Partnership Agreement Signing Ceremony
(Right:
  Masato Maedomari, Mayor of Taketomi Town, Okinawa
 Left:
  Hideki Umemoto, General Manager of
  the Green Energy Products Unit,
  Innovation & Business Development HQ, NTN)
Photo:“N3 N-CUBE” Restroom Model Installed at Oomija Road Park on Iriomote Island, Taketomi Town “N3 N-CUBE” Restroom Model Installed at
Oomija Road Park on Iriomote Island,
Taketomi Town

Figure:Taketomi Town consists of multiple remote islands, including Iriomote Island. Taketomi Town consists of multiple remote islands, including Iriomote Island.

Transportable Independent Power Supply “N3 N-CUBE”

“N3 N-CUBE” is a Transportable Independent Power Supply that operates solely on renewable energy generated by wind turbines and solar panels. Featuring high mobility, it can be rapidly transported and installed where it is needed. The interior space of the container can be flexibly utilized for a variety of purposes, including restrooms and multipurpose spaces.

Related Links

Photo:Transportable Independent Power Supply “N3 N-CUBE”

“N3 N-CUBE” Restroom Model

The “N3 N-CUBE” Restroom Model incorporates a self-contained circulation type flush toilet system. The container is equipped with both a toilet unit and a treatment tank that decomposes and purifies wastewater. Wastewater generated after use is treated within the container and reused as flushing water, eliminating the need for external water supply or sewage infrastructure. Powered by electricity generated from solar panels and wind turbines, the system provides a clean and sanitary restroom environment even in locations where access to electricity and water is difficult, such as disaster-affected areas, temporary facilities, and tourist destinations.

Photo:“N3 N-CUBE” Restroom Model

Since its installation on Iriomote Island in May 2025, the “N3 N-CUBE” Restroom Model has improved convenience for both residents and tourists. It has been highly regarded for its environmental performance as a renewable-powered system, as well as for its ability to be deployed in a wide range of locations, rapid deployment, and cost-effectiveness achieved without the need for infrastructure development.

Related Links

Inquiries about this release

Inquiry Form

Print