HOME > Product and Technology > Products News : 2026 >  Transportable Independent Power Supply “N3 N-CUBE” Adopted at 11 Locations Nationwide, Including Disaster-Resilient Roadside Stations

2026

Transportable Independent Power Supply “N3 N-CUBE” Adopted at 11 Locations Nationwide, Including Disaster-Resilient Roadside Stations May 21, 2026 Products News

  • Operating on 100% renewable energy and functioning as a disaster-relief container toilet usable during power and water outages

NTN Corporation (hereafter, NTN) has had its Transportable Independent Power Supply “N3 N-CUBE” adopted as a disaster-relief container toilet at Disaster-Resilient Roadside Stations (Michi-no-Eki) designated by Japan's Ministry of Land, Infrastructure, Transport and Tourism (MLIT). To date, a total of 11 units has been installed nationwide

Disaster-resilient roadside stations are facilities selected by MLIT from among roadside stations across Japan to serve as wide-area disaster response hubs, providing logistical support and assistance to evacuees in the event of large-scale disasters.

Following the initial installation of one “N3 N-CUBE” unit as a disaster-relief container toilet at the Disaster-Resilient Roadside Station “Shimotsuke” in Tochigi Prefecture*1, installations were gradually expanded in various regions. As a result, 11 units have now been installed across the Kanto, Kinki, and Kyushu regions.

The adopted “N3 N-CUBE” is equipped with a fully self-contained, water-circulation flush toilet system featuring a wastewater treatment tank. As it does not require external water supply or drainage infrastructure, the system can maintain a clean and sanitary restroom environment regardless of installation location. In addition, the system operates on 100% renewable energy generated by solar panels, allowing continued use even during power outages or water supply disruptions. Its high mobility enables transportation by truck, providing both a stable power supply and a sanitary restroom environment even in locations without established electricity or water infrastructure. Furthermore, the “N3 N-CUBE” is scheduled to be operated as a phase-free disaster prevention facility, enabling use both during normal times—such as at roadside stations—and in the event of a disaster, when it can be relocated to affected areas as needed.

NTN will continue to expand the deployment of independent power supply systems utilizing renewable energy, including the “N3 N-CUBE”, across a wide range of applications. Through these efforts, NTN aims to contribute to sustainable growth and to the resolution of social issues.

  1. Press release on March 10, 2026:
    Transportable Independent Power Supply “N3 N-CUBE” Adopted as a Disaster-Relief Container Toilet at the Disaster-Resilient Roadside Station “Shimotsuke”
    https://www.ntnglobal.com/en/news/new_products/news202600014.html
Photo:Transportable Independent Power Supply “N3 N-CUBE” installed at the disaster-resilient roadside station “Tajima no Mahoroba.” Transportable Independent Power Supply
“N3 N-CUBE” installed at the disaster-resilient
roadside station “Tajima no Mahoroba.”
Photo:Equipped with two Western-style toilets and a treatment tank, it provides a clean and sanitary restroom environment Equipped with two Western-style
toilets and a treatment tank,
it provides a clean and
sanitary restroom environment
Photo:At the disaster-resilient roadside station “Yufuin” in Oita Prefecture, the “N3 N-CUBE” features an exterior design that blends in with the surrounding landscape At the disaster-resilient roadside station
“Yufuin” in Oita Prefecture, the “N3 N-CUBE”
features an exterior design that blends
in with the surrounding landscape

Installation Site

Figure:Installation Site

No. (map) region Address Installation Site
① *2 Kanto region Shimotsuke City,
Tochigi Prefecture
Roadside Station
“Shimotsuke”
② Kinki region Nagahama City,
Shiga Prefecture
Roadside Station
“Shiotsukaidou Adikamanosato”
③ Kyotanba Town,
Kyoto Prefecture
Roadside Station “Nagomi”
④ Nara City,
Nara Prefecture
Roadside Station “Hari T・R・S”
⑤ *2 Susami Town,
Wakayama Prefecture
Roadside Station “Susami”
⑥ *2 Takahama Town,
Fukui Prefecture
Roadside Station
“Seaside Takahama”
⑦ *2 Asago City,
Hyogo Prefecture
Roadside Station
“Tajima no Mahoroba”
⑧ *2 Kyusyu region Yufu City,
Oita Prefecture
Roadside Station “Yufuin”
⑨ *2 Ashikita Town,
Ashikita District,
Kumamoto Prefecture
Roadside Station “Tanoura”
⑩ *2 Miyakonojo City,
Miyazaki Prefecture
Roadside Station “Miyakonojo NiQLL”
⑪ *2 Tarumizu City,
Kagoshima Prefecture
Roadside Station “Tarumizu Hamabira”
  1. Disaster-resilient roadside stations designated by the Ministry of Land, Infrastructure, Transport and Tourism

Transportable Independent Power Supply “N3 N-CUBE”

The “N3 N-CUBE” is a transportable independent power supply equipped with a wind turbine and solar panels, enabling rapid transportation to locations where it is needed. The interior space of the container can be flexibly utilized according to its purpose, allowing deployment in a wide range of applications, including restrooms and multipurpose spaces.

Photo:Transportable Independent Power Supply “N3 N-CUBE”

“N3 N-CUBE” Restroom Model

The container is equipped with both the toilet unit and a wastewater treatment tank that breaks down and purifies sewage. Through biological treatment, the processed wastewater is reused as flushing water, eliminating the need for external water supply or drainage infrastructure. The system operates using electricity generated by solar panels and other renewable energy sources, suppressing odors while providing a stable and sanitary restroom environment even during disasters or in locations with infrastructure constraints, such as temporary facilities and tourist destinations.

Inquiries about this release

Inquiry Form

Print