HOME > Product and Technology > New Products : 2025 >  NTS Develops Picking Feeder “ROBOCLE”

2025

NTS Develops Picking Feeder “ROBOCLE” November 26, 2025 New Products

  • Combining space-saving design and high-speed performance, enabling easy automated picking without specialized knowledge
  • Contributing to automated picking in manufacturing sites with three types of picking feeders: “TRINITTE,” “ROBOCLE,” and “CHOXY”

NTN Technical Service Corporation (hereafter, NTS), a consolidated subsidiary of NTN Corporation (hereafter, NTN) announces the launch of “ROBOCLE,”*1 a parts feeder developed by NTS for use in machining and assembly processes at manufacturing sites. This product combines a space-saving design with high-speed performance. “ROBOCLE” reduces installation space and enables automatic picking of various workpiece shapes without requiring specialized knowledge. It achieves this by integrating a newly developed picking actuator with “TRINITTE,”*2 originally developed in 2021.

NTS will continue to offer three types of picking feeders: the existing high-speed model “TRINITTE,” the space-saving model “CHOXY,”*3 and the new model “ROBOCLE,” which combines the strengths of both. Through these solutions, we aim to contribute to labor-saving and efficiency improvements in manufacturing sites.

  1. The name symbolically represents the synchronized motion of the robot and disc sharing the same rotational axis. It combines “robot” and “circle,” reflecting the concept of circular rotation.
  2. Press release on September 29, 2021:
    Developed the picking feeder for robots, “TRINITTE”(only in Japanese)
    https://www.ntn.co.jp/japan/news/new_products/news202100063.html
  3. A stylish name inspired by the characteristics of “straight movement” and “straight line.”

Development background and overview of “TRINITTE”

In response to a declining labor force and growing demand for higher productivity, manufacturing sites are advancing the automation of picking operations, such as workpiece loading and alignment. Since the 1970s, NTN has been developing and selling parts feeders for supplying workpieces to processing machines and today holds one of the leading market shares in Japan.

Conventional parts feeders require setup changes according to workpiece shape. However, as multi-variety, small-lot production becomes more common, there has been growing demand for parts feeders capable of picking diverse workpieces without setup changes. To meet this need, NTS developed the picking feeder for robots, “TRINITTE,” in 2021. TRINITTE places workpieces on a rotating disc and integrates a camera with a picking robot, enabling stable picking regardless of workpiece shape or orientation. The system is now being adopted in various fields including electronic components and automotive parts.

Photo:Configuration of “TRINITTE” Configuration of “TRINITTE”

Although “TRINITTE” has received high praise, the space required to install the picking robot, the need for a robot with sufficient capability, and specialized knowledge for robot teaching have been barriers to adoption. To provide more customers with the same capability for automatic picking of diverse workpieces as “TRINITTE,” we have now developed “ROBOCLE,” which offers space-saving and enhanced usability.

Overview of “ROBOCLE”

“ROBOCLE” is a picking feeder that combines “TRINITTE” with a newly developed picking actuator. It is the ideal solution for customers who found it challenging to adopt the conventional configuration of “TRINITTE” with a picking robot due to the required installation space and the need for specialized knowledge of robot teaching.

Unlike “TRINITTE,” which places the picking robot around the main unit, “ROBOCLE” mounts the newly developed actuator at the center of the unit, reducing installation space by approximately 25% while ensuring smooth picking. In addition, its dedicated user interface enables easy teaching without specialized knowledge.

Photo:Configuration of “ROBOCLE” Configuration of “ROBOCLE”

Features of “ROBOCLE”

1. Space-saving design Adopts a design that places a picking actuator around the system's center
Allows space-saving installation without the need to mount picking robots such as industrial or collaborative robots around TRINITTE
Compared to a setup combining TRINITTE with picking robots (including robot operating range), installation space is reduced by approximately 25%
2. High-speed operation The synchronized “Rotating and Picking” motion delivers smooth, efficient picking
The minimum cycle time from pick to place is approximately 2 seconds
3. Easy setup An easy-to-use picking system designed for on-site operations, requiring no advanced robotics knowledge or skills
A dedicated user interface makes configuration simple and intuitive

Overview of “CHOXY”

“CHOXY” is a picking feeder that combines the “Mono-Drive Two-Way Feeder”*4 (with a proven track record of over 5,000 units delivered), a linear conveyor, and a picking robot. Compared to “TRINITTE” and “ROBOCLE,” it offers the most space-saving design and the simplest setup, making it ideal for customers looking to easily automate picking.

In “CHOXY,” a single linear feeder first accurately aligns the workpieces, then transfers them via a linear conveyor to the collaborative robot or other robot, the robot picks them up. Switching between workpiece types and operation modes is also simple, allowing users to install and operate the system without specialized knowledge.

  1. A compact return feeder that enables storage, alignment, and supply with a single linear feeder.

Photo:“Mono-Drive Two-Way Feeder” “Mono-Drive Two-Way Feeder”

Photo:Configuration of “CHOXY” Configuration of “CHOXY”

Features of “CHOXY”

1. Simple configuration A cost-effective picking system combining the “Mono-Drive Two-Way Feeder,” a linear conveyor, and a picking robot
2. Space-saving design A compact product configuration that reduces installation space requirements
3. Support for user self-operation Simple structure and settings allow users to operate the system themselves without requiring specialized knowledge

NTS offers three types of picking feeders—“TRINITTE,” “ROBOCLE,” and “CHOXY”—to deliver optimal solutions tailored to customers' environments and needs, contributing to automated picking of various workpieces and to labor-saving and efficiency improvements in manufacturing sites.

These three picking feeders will be showcased at the “2025 International Robot Exhibition,” held at Tokyo Big Sight in Japan from December 3 to 6.

Picking feeder product lineup

TRINITTE ROBOCLE CHOXY
Appearance Photo:TRINITTE Photo:ROBOCLE Photo:CHOXY
Configuration TRINITTE
+
Picking robot
TRINITTE
+
Picking actuator
Mono-Drive Two-Way Feeder
+
Linear conveyor
+
Picking robot
Concept
  • The “Trinity” structure of the Vibrator, Bowl, and Disc integrates feeding, alignment, and picking into a single system.
  • With arc conveyor tracking technology, the robot can follow workpieces moving along an arc, enabling stable and continuous picking.
  • A space-saving and efficient picking solution achieved through a design that places a picking actuator at the center of the feeder.
  • An easy-to-use picking system that can be operated without advanced robotics knowledge, ideal for on-site applications.
  • Simple picking system
  • Compact design for space-saving
  • Enables user self-operation
Application
  • Assembly, processing, and palletizing (arrangement) of small workpieces
  • Inspection using TRINITTE+camera(OK/NG judgement)
  • Small-lot, multi-variety roduction
  • Specific processes within line production
  • Assembly, processing, and palletizing (arrangement) of small workpieces
  • Pre-processing and positioning of integrated molded workpieces for assembly and machining
  • Standalone operation with an independent machine
  • Alignment and positioning of small workpieces
  • Automatic placement of small-lot workpieces
  • Palletizing (arrangement) of assembly components
  • Counting-based feeding
  • On-site assistance close to the operator
Space-saving ★ ★★ ★★★
Cycle time ★★★ ★★ ★
Ease of implementation*5 ★ ★★★ ★★★
Impementation cost*6 ★ ★★ ★★★
  1. Programming language knowledge required for teaching a picking robot
  2. Cost required for implementing a picking feeder system
★
Inferior
Figure:↔
★★★
Superior

Inquiries about this release

Inquiry Form

Print