HOME > Product and Technology > New Products : 2025 >  NTN Starts Proposals of “HA-C Bearing” with Industry's Highest Level in High Load Capacity Achieved by Special Heat Treatment Technology to Automobiles

2025

NTN Starts Proposals of “HA-C Bearing” with Industry's Highest Level in High Load Capacity Achieved by Special Heat Treatment Technology to Automobiles May 20, 2025

  • Achieving downsizing, lightening, dimensional stability at high temperature, contaminated lubrication resistance, and wear resistance of bearings
  • Proposing to automotive applications such as e-Axles for EVs and HEVs, transmissions for HEVs and internal combustion engine vehicles, and compressors

NTN Corporation (hereafter, NTN) starts proposals of the “HA-C*1,2 Bearing” in which NTN's proprietary special heat treatment technology “HA-C” is applied to deep groove ball bearings, to markets such as automobiles.

The “HA-C Bearing” enables downsizing and lightening of bearings by the “HA-C” which realizes the industry's highest level in high load capacity. We will propose this product to a wide range of automotive applications such as e-Axles, which is a drive source for electric vehicles (EVs) and hybrid electric vehicles (HEVs), transmissions for HEVs and internal combustion engine vehicles, and compressors, contributing to energy saving in various types of vehicles.

  1. HA-C: High Antiwear and Capacity
  2. Press release on May 20, 2024:
    NTN Develops Special Heat Treatment Technology “HA-C,” Contributing to Downsizing and Lightening of Drive Units for Automobiles
    https://www.ntnglobal.com/en/news/new_products/news202400033.html
Photo:Comparison of dimensions between “HA-C Bearing (left)” and conventional product (right) Comparison of dimensions
between “HA-C Bearing (left)”
and conventional product (right)
Figure:Example of applied areas in parallel axis e-Axle (red circle) Example of applied areas in parallel axis
e-Axle (red circle)

The “HA-C” is NTN's proprietary special heat treatment technology that uses a large number of hard and fine precipitates to disperse, resulting in extremely high surface hardness and high load capacity.

By adopting the “HA-C,” the “HA-C Bearing” can achieve approx. 15% downsizing in outer diameter, approx. 30% downsizing in width, and approx. 55% lightening*3, while maintaining the same bearing operating life compared to the conventional product. It responds to the needs for more compact and lighter bearings used in various automotive drive units such as e-Axles and transmissions towards improvements in fuel and electricity efficiency.

In order to improve fuel and electricity efficiency, lubricating oil used in drive units also tends to be low viscosity to reduce frictional resistance. Under the usage conditions, each part of the bearing is more likely to come into direct contact with each other, thus the operating life of the bearing is reduced and wear is more likely to occur. In addition, contamination lubrication in the drive units may enter the bearings and damage them. As the “HA-C Bearing” achieves high levels of contaminated lubrication resistance and wear resistance in addition to long bearing operating life, it can be used in these harsh usage conditions.

  1. For catalog standard series. Size can be further reduced by special design.

Since announcement of the development of this technology in May 2024, NTN has received many inquiries and requests from customers regarding the application of the “HA-C” to make bearings more compact, lighter, and longer operating life, and has been preparing for the mass-production of this bearing. After repeated performance verification, we have decided to start proposals of the “HA-C Bearing.”

NTN will propose the “HA-C Bearing” as the most suitable product for downsizing, lightening, and efficiency improvement in various automotive applications such as e-Axles, contributing to further energy saving in automobiles. NTN will also promote the development and proposal of this product to a wide range of industries other than automobiles, taking advantage of features such as compactness, lightweight, and wear resistance.

NTN will exhibit the developed high performance model of “EDJ” at the “Automotive Engineering Exposition 2025 YOKOHAMA” to be held from May 21 to 23 at PACIFICO Yokohama in Japan.

Features (compared to standard type bearing)

1. High load capacity Increase static load capacity by 2 times and improve rolling fatigue life under heavy load conditions by more than 8 times*4.
Improving high load capacity enables to replace bearings with more compact and lighter ones
(Replacement example: approx. 15% downsizing in outer diameter, approx. 30% downsizing in width, and approx. 55% lightening*3)
2. Contaminated lubrication resistance Improve rolling fatigue life under contaminated lubrication with debris by more than 4 times*4
3. Dimensional stability at high temperature Suppress dimensional change at 150℃ to less than 1/2
4. Wear resistance Reduce the amount of wear to less than 1/300*5
  1. Due to additional performance verification, the figures have been revised upward from the time of the development announcement of *2
  2. Based on NTN's test under lubricating conditions where oil film is difficult to form

Applications

e-Axles, transmissions, compressors, etc.

Inquiries about this release

Inquiry Form

Print