|

|
New SMD Feeders Announced
NTN has developed two new SMD Feeders: One is a SMD Feeder with Image
Processor. This high speed unit was developed for aligning micro-electronic
components with their correct sides facing upward and forward to the next
processing device with the highest precision. The second new SMD Feeder
has an auto-eject mechanism. This new unit was developed for use in aligning
resin based components and is capable of automatically ejecting off-line
components in its parts feeding process with the fastest supply speed
in the industry
1.Development Background
Electronic assembly often requires the alignment of micro-electronic
components with both their correct sides facing upward and forward. However,
the number of components with the identification mark too small to tell
which is back and forward is increasing. These components require the
use of an image processor for their alignment. The precision of existing
SMD feeders with image processors, prior to the new NTN unit, is relatively
low. Accordingly, the market is in need of a SMD feeder with both a high
precision and high speed image processor.
It has also been observed in the manufacturing process of chip Light-Emitting
Diodes, as used in external illuminants for LCD displays for example,
that trouble often occurs within the parts feeder due to minute external
weld flashes. This has been seen in the high precision alignment of resin
based parts where static electricity often occurs. This has led to a lowered
production rate.
2. Outline of Product
1) SMD Feeder with Image Processor
Target Parts: Micro electronic components that require the correct sides
facing upward and forward, but the identification mark is not large
enough to recognize with standard SMD feeders.
Through the addition of new NTN technology, a new proprietary mechanism
(patent pending)for processing micro electronic components with minute
identification marks at high-speed. Through this NTN has achieved
the highest level of high precision alignment and high-speed supply
in the industry. We have created a machine of simple construction
and high durability by simply employing NTN's proprietary alignment
mechanism and image processing.
2) SMD Feeder with Auto-eject Mechanism
Target Parts: Resin based small electronic components
NTN has developed an automatic ejection mechanism which ejects off-line
parts out of the parts feeder, resulting in drastically improving
production rate. NTN has succeeded in employing measures to neutralize
static electricity with ionized air, and a straight feeder alignment
style, creating reliable aligned supply to the world's highest standard.
3. Features
1) SMD Feeder with Image Processor
- High precision alignment and high-speed supply: 99.99% precision
alignment, and high-speed supply of up to 400-units/ minute. (1608
size.)
- Simple mechanism of high durability
- Adapts to any identification mark with the press of a button
2) SMD Feeder with Auto-eject Mechanism
- An extremely high utilization rate of 99.99%
- World's highest speed supply capability of 1500-units/ minute. (LED
1608 chip),
- Compact (3/4 of machine to date)
4. Target Parts
- SMD Feeder with Image Processor
Chip parts polarized to forward and backward
-
SMD Feeder with Auto-eject Mechanism
Resin based SMD parts such as chip LED, CR filters, EMI filters,
and Tantalum condensers, where the dimensional precision of external
markings is difficult to discern. Also work where static electricity
occurs easily.
5. Sales Volume: 5 billion yen yearly
SMD Feeder with Image Processor
 |
SMD Feeder with Auto-eject Mechanism
 |
|