NTN Exhibits at “EMO Hannover 2019”September 4, 2019
| Date | September 16 (Mon) to 21 (Sat), 2019 |
|---|---|
| Venue | Hanover Fairground (Hanover, Germany) |
| Booth No. | Hall7 D10 |

NTN Corporation (hereafter, NTN) will exhibit at the machine tool-related exhibition “EMO Hannover 2019” held in Hanover, Germany from September 16 to 21.
In adittion to the main theme of “Navigate Your Future -NTN ULTAGE*” four sub-themes, namely, “Machine Tools”, “Robotics,” “Linear,” and “Training and services” will be set and products will be exhibited according to the theme.
At the booth, NTN will exhibit products such as precision bearings for machine tools that are equipped with high-performance such as realizing both high speed rotational performance and high-load capacity as well as sensing, and bearings for multijoint robot gearboxes. NTN will also introduce the “i-WRIST™” Wrist Joint Module, which enables smooth and quick movement, linear modules for direct guidance of the machine, and maintenance tools such as “SmartTEMP,” an induction heater for attaching mechanical components including bearings to machinery.
We look forward to seeing you all at the event.
* ULTAGE is the name for NTN's goal of achieving the ultimate performance with precision bearings, and expresses the “Ultimate” performance on any type of “Stage.”
Main exhibits