NTN Exhibits at the “SIMTOS 2016 (17th Seoul International Manufacturing Technology Show)”April 4, 2016
| Date | April 13 (Wed) to 17 (Sun), 2016 |
|---|---|
| Venue | KINTEX Goyang, Korea |
| Booth No. | Hall 1 02B960 |

NTN will run a booth at the “SIMTOS 2016 (17th Seoul International Manufacturing Technology Show)” with the theme “Core Technology of Machine Tools, NTN,”with numerous exhibits including the ULTAGE* series of bearings as well as other products for machine tools.
Dynamic exhibits of linear modules will also be on show, and the booth will feature demonstrations of the Bearing Technical Calculation System for Machine Tool Spindles and maintenance tools.
We look forward to seeing you at the event.
* ULTAGE is the name for NTN's new generation of the world's highest standard of bearing series, and expresses the [ULTIMATE] performance on any type of [STAGE.] It represents NTN's goal of achieving the ultimate performance with precision bearings.
Main exhibits
ULTAGE series of precision rolling bearings for machine toolsPrecision bearings responding to the need for improved efficiency, reliability, quality and environmental responsibility for machine tools. Optimization of the bearing's internal design, as well as special material and surface improvements, special grease and the use of seals on both sides deliver outstanding performance. |
|
Machine Tool Main Spindle Bearing with Air Cooling SpacerReduces the difference in temperature between the inner and outer rings with the use of an “air cooling spacer” using proprietary air cooling technology suited to bearing for main spindle of machine tools. This improves the high-speed rotational performance by 20% compared to conventional products (High-speed Angular Contact Ball Bearings), and achieves a dmn value of 2.1 million to achieve the world's highest standard high-speed rotational performance with air-oil lubrication and fixed-position preload. |
|
Bearing Technical Calculation System for Machine Tool SpindlesDesigned for precision rolling bearings used for machine tool spindles, this system that allows customers to quickly and automatically calculate main shaft rigidity, bearing operating life and other features. 10 types of main shaft patterns can be calculated, and the dedicated server operates 24 hours a day, 365 days a year for use at any time. |
Ball Screw Support UnitDelivers the world's highest load capacity as a ball screw support unit, and uses a newly developed seal for low torque and high dust proofing. Comes filled with a long-life grease initially, eliminating the need for additional lubrication. |
|
Linear moduleLinear motion units, which have small to large sized aluminum frames to special lightweight designs, are deployed with high-performance guide installed. The optimal type, size, stroke and drive method to suit applications such as processing machinery, work loaders of assembling machinery, and positioning equipment can be selected, while multiple units can be combined for a multi-axis layout in the X/Y/Z directions. |
|
Maintenance toolA support tool to make work pressing and pulling bearings by customers at machinery maintenance and repair sites. |
|