NTN Exhibits at the European Mechatronics Meeting (EMM) 2012June 7, 2012
| Date | June 6 (Wed) to 7 (Thu), 2012 |
|---|---|
| Venue | Le Grand-Bornand, Haute-Savoie, France |
NTN-SNR will be exhibiting at the European Mechatronics Meeting (EMM) 2012. In addition to a technical presentation (to be held on June 7) on EV system products utilizing NTN-SNR's sensor and control technology, there will be dynamic exhibits of the four-wheel electric commuter “Q'mo,” the In-Wheel Motor System and One Motor Type Electric Vehicle Drive System. We look forward to seeing you at the event.
Main Products
In-Wheel Motor Systemand Compact EV Chassis Model
A compact in-wheel motor that utilizes a thin hub bearing, reducer and motor, which can be mounted within small diameter wheels of commuters. The system also includes a drive motor, reducer, hub bearing and inverter for advanced vehicle control.
In-Wheel Motor System and Compact EV Chassis Model
One Motor Type Electric Vehicle Drive System
Coordinated control of the vehicle drive motor and gear actuator allow faster, smoother gear changes, while selection of the most appropriate gear ratio to suit the vehicle's driving conditions provides smooth acceleration, even with a lightweight drive motor. Selection of the most appropriate gear ratio ensures high-speed driving, as well as increasing the driving mileage available from a single charge.