NTN participates in China Wind Power 2010 expositionDecember 28, 2010
NTN entered China Wind Power 2010, the largest exhibition of the kind in China, for the first time so as to have its contribution to generating clean power better known in China. During the exhibition, held at the China International Exhibition Center New Venue in Beijing from October 13 to 15, NTN set up its own booth under a theme, “Ready to Protect the Environment”, and in its bearings supporting clean energy, publicized that NTN is ready to supply any types of bearings in any size required for wind power plants. The booth displayed real bearings for gearbox and for power generator and a large spherical roller bearing for main shafts, as well as an extra-large double-row tapered roller bearing reproduced by computer graphics in life size on a panel.
Power generator bearing (extreme left) and bearings for gearbox (center)
A main shaft bearing on display (right) and a panel showing a life-size illustration of an extra-large double-row tapered roller bearing