Development of “Tapered Roller Bearings” with an early failure detection functionJune 30, 2016
Enables early detection of bearing peeling. Also prevents fragment dispersion should flaking occur
NTN Corporation (hereafter, NTN) has developed “Tapered Roller Bearings” with an early failure detection function which can detect flaking that occurs on bearings during operation.
Continuous use of bearings with flaking failure leads to a risk of damage to peripheral components such as the shaft and housing due to abnormal bearing rotation. Furthermore, this will also cause secondary damage such as damage to gear parts when flaked fragments from bearings are dispersed and become stuck in the gears. Therefore, when flaking occurs on bearings, it is best to stop operation promptly. However, until now, it was difficult to detect flaking on bearings because it was undetectable due to the vibrations or noise of the entire machine.
On the other hand, it is necessary to have a replacement period for bearings as long as possible to reduce the life cycle cost of the machine. However, because the risk of bearing damage including secondary damage increases the longer the replacement period, so that the actual bearing replacement period is usually set to a much shorter period than the expected operating life of bearings from the perspective of risk reduction.
Due to these factors, there has been a need for technology to detect flaking on bearings in the early stages and for technology to reduce the possibility of secondary damage due to flaking as much as possible.
NTN has developed a product that prevents flaking fragments from being discharged outside of the bearing by installing a filter seal on the outer ring, which is a stationary ring on the tapered roller bearings, and by optimizing the clearance between the inner ring and filter seal. Also, by optimizing the sensitivity of the damage detection sensor attached to the filter seal, NTN has achieved a technology that can detect whether flaking only has occurred at an early stage without detecting fine iron powder or suspended metal particles. In addition, the filter seal has a special construction that also allows it to be retrofitted to existing tapered roller bearings.
NTN will propose this technology over a wide area for tapered roller bearings used on machines in the general industry and continue to contribute to reducing the life cycle cost of machines.
Features
(1) Can detect flaking on tapered roller bearings at an early stage | Detects flaking using a damage detection sensor |
---|---|
(2) Reduces the possibility of secondary damage occurring due to flaking on bearings | Controls the dispersion of flaking fragments using a filter seal and prevents secondary damage to peripheral components |
(3) Can install on existing bearings | Can be installed without any dimension changes onto existing bearings because of its parted construction |
Application
Construction machinery
Inquiries about this release
Product photos
Construction