HOME > News > Event : 2024 > NTN Exhibits at “RoboDEX – The 8th Robot Development & Application Expo”

2024

NTN Exhibits at “RoboDEX – The 8th Robot Development & Application Expo”January 18, 2024Event

Exhibiting the products that contribute to labor saving and automation at manufacturing sites and improving the performance of industrial robots

Date January 24 (Wed) to 26 (Fri), 2024
Venue Tokyo Big Sight
(3-11-1 Ariake, Koto-ku, Tokyo)
Booth No. W54-64

Photo:“RoboDEX – The 8th Robot Development & Application Expo”

NTN Corporation (hereafter, NTN) exhibits at “RoboDEX – The 8th Robot Development & Application Expo” held from January 24 to 26, in Tokyo Big Sight, Tokyo, Japan.

This event is a specialized robot exhibition where robot development technologies including the latest robots and peripheral equipment gather. This time, approx. 1,650 related companies that deal with robots for factories, logistics, and services, as well as robot-related parts will exhibit the latest technology.

In recent years, while the demands for labor saving and streamlining at manufacturing sites is growing, NTN will introduce products that contribute to the automation of manufacturing sites, such as “Microscopic Coating Applicator” that applies extremely small amounts of liquids of various viscosities at high speed and with high precision, Wrist Joint Module “i-WRIST™” that enables high speed positioning with a smooth movement, and other products.

We look forward to seeing you at the event.

Main exhibits

“Microscopic Coating Applicator”

This is a device that applies liquid of various viscosities of several pl (one trillionth of a liter) adhered to the tip of a needle with high precision in 0.1 second per application. It applies the technology of repair equipment that repairs minute defects in LCD panels and color filters, this device can be applied to chip components and micromachine adhesive application, as well as to life science-related applications such as the development of three-dimensional cell chips.

At this exhibition, we will demonstrate the actual application operation.

Photo:“Microscopic Coating Applicator”

Wrist Joint Module “i-WRIST™”

It is a compact positioning module that achieves a wide range of angle movement while saving space. This can move smoothly like human wrist at high speed to perform minor position (angle) changes, which vertically articulated robots are not good at doing.

The maximum weight capacity is 3kg. It adapts to various mounting postures including upward, sideways, and inclined directions. By attaching end effectors such as camera, lightning, dispenser, and cleaning nozzle, it can contribute to automation, improvement in efficiency, and saving labor of various processes such as appearance inspection, grease dispensing, and cleaning.

At this event, we will exhibit “i-WRIST” Starter Package which includes the main unit and peripheral parts, as well as demonstration machines for visual inspection and grease application.

Photo:Wrist Joint Module “i-WRIST™”

Inquiries about this release

Inquiry Form

Print